JUMP TO CONTENT

CHIPLET Device Development, CHIPLET Installed System Development Engineer

この欠員は期限切れです。 下の同様の職務を参照してください...


Job Description

【Reason for Hiring】

SoC products for automotive applications are key parts for realizing the digitization and higher functionality of automobiles, and their evolution is unstoppable. In recent years, higher performance and higher functionality have been realized, and package substrates and application boards are required to meet advanced requirements (e.g., suppression of transmission loss and noise, assurance of signal quality, etc.).
This work involves circuit and artwork design and verification through simulation of signal quality in order to realize PCB boards for package and application systems that meet these requirements. 

【Role Responsibilities】

Development of chiplet devices and system modules using chiplet technology

  • Define the architecture of a chiplet device system module
  • Specify the outline of the circuit/artwork and define the verification method for it
  • Lead the development of interposer design to achieve the above interface and power specifications
  • Consideration of system board specifications for evaluating development devices
  • Communicate engineers who design circuit and artwork
  • Write detailed technical reports on development outputs

*The full details regarding your position scope as well as any future potential changes in work location and job scope will be provided during the interview process.

【What We Offer】

This technology is central to the realization of large-scale systems using chiplets and multi-chip modules, which will improve significantly in the future, and this position will allow the candidate to learn a highly promising technology.

What Are We Looking For

We are looking for individuals who are passionate about new technologies and eager to collaborate with us, particularly in the area of chiplets. We value motivation and skills over language proficiency. Proficiency in either Japanese or English is required.


Qualifications

【MUST】

  • Knowledge of PCB board circuit/artwork design for semiconductor system boards
  • Experience with simulation tools to perform signal quality evaluations
  • Experience for the circuit design of system level board
  • Proficiency speaking in either Japanese or English

【WANT】

  • Knowledge of phenomena that affect signal quality, such as transmission loss, reflections, and crosstalk
  • Fundamental knowledge about memory devices and interfaces such as DDR, Flash, NVM is plus
  • Fundamental knowledge about standards of communication interfaces such as MIPI, PCIe, and else is plus
  • Fundamental knowledge in the electrical circuit of digital and analog

Additional Information

Recruiter : Masana Ueno

ルネサスは、「To Make Our Lives Easier 」(人々の暮らしを楽“ラク”にする)というPurposeの下、組み込み半導体ソリューションを提供します。高品質とシステムレベルノウハウを兼ね備えた組み込み半導体のリーダーとして、自動車、産業、インフラ・IoT分野向けに、ハイパフォーマンスコンピューティング、組み込みプロセッシング、アナログ&コネクティビティ、そしてパワーを含めた幅広い製品ポートフォリオを軸とした、スケーラブルで包括的なソリューションを提供しています。
 

ルネサスは、30か国以上で21,000 人を超える多様性あふれる従業員と共に、限界に挑戦しながら、デジタライゼーションを通じてユーザエクスペリエンスを充実化させ、新たなイノベーションの時代を切り開いていきます。そして世界中の人々やコミュニティの未来のために、持続可能で省エネ効果の高いソリューションの開発に全力で取り組み、「To Make Our Lives Easier」を実現します。    
 

ルネサスで実現できること
 

  • キャリアをスタート、そしてキャリアアップ:4つのプロダクトグループをはじめ、さまざまな部門において技術職として、また幅広いビジネスの経験を積むことができます。ハードウェア、ソフトウェアの専門知識を深めたり、新しいことにチャレンジしたりする機会があります。 
     
  • やりがいとインパクトのある仕事をする: 革新的な製品とソリューションの開発に関わることにより、世界中のお客様のニーズに応えると同時に、人々の生活をより便利で安全かつ安心なものにすることに貢献できます。
     
  • 「ウェルビーイング」に焦点を置いた環境で最大限に能力を発揮する:ルネサスでは、リモートワーク制度などによる柔軟な勤務体制づくり、また従業員リソースグループの積極的な活動をサポートするなど、インクルーシブな職場環境構築を目指しています。従業員を第一に考えたカルチャーとグローバルなサポート体制が、入社後すぐに活躍できる環境を提供します。 

 

自分の力で成功を掴み、キャリアを築く準備はできていますか? 

ルネサスで一緒に未来を形づくっていきましょう

  1. エンジニア
  2. 小平市
  3. No

求人ID

20018130_2024-12-06

職種検索

Browse Jobs