Sr Staff Analog Engineer
この欠員は期限切れです。 下の同様の職務を参照してください...
【Background】
This team support SPS FET design for PCP. In the last year, two out of the four device engineers who no longer with the company. We are aslo supporting the new MV FET REXFET2 and REXFET3. The SPS FETs are critical for PCP and we enetering a period of incredible growth for SPS FETs where we are looking at volume sales increasing by 3x in the next 2 years.
【Job Description】
We are seeking a Sr. Staff Design Engineer to develop cutting edge switching power MOSFETs for 12V to 80V applications. You will participate in the full product cycle from conception of architecture through final product characterization. This will involve the conception and development of novel power MOSFET device structures, optimizing those structures for performance and ruggedness, and developing test and characterization methods to demonstrate device capability and limits. You will work in a team of highly experienced device and process integration engineers to develop cost-effective, manufacturable devices for some of the most demanding of power applications. This is a high visibility position with potential to make significant business and technological impacts.
- Develop novel, high-performance, high-reliability power switching device technology for one of our fast-growing business units
- Work closely with process engineers toward development of new process flows and design rules
- Design and execute TCAD simulation experiments to center critical process and design parameters
- Identify critical design parameters and process sensitivities which affect yield to pre-defined specifications
- Collaborate with internal CAD and layout teams to develop test mask and product mask layouts and parameterized cells (P-Cells)
- Design and analyze process and design of split experiments
- Work closely with applications and test engineers to gather characterization data and ensure robust test methodologies
- Help identify testing requirements for new technologies based on specific device architectures and application stresses
- Analyze measured device and test structure data to solve problems and optimize device design and process
- Provide engineering support for existing power semiconductor products
*The full details regarding your position scope as well as any future potential changes in work location and job scope will be provided during the interview process.
【MUST】
- Semiconductor Device Physics / Solid State Physics
- Semiconductor Device Process Integration
- TCAD process and device simulation (preferably Sentaurus)
- Conversational proficiency in English
- Business-level proficiency in Japanese
【 WANT/ Nice-to-Have 】
- Product and test mask layout (preferably Cadence Virtuoso)
- Design of Experiments methodology
- Working familiarity with structural and chemical analysis for microelectronics
- Working familiarity with power device test and characterization equipment and methodologies
- Understanding of switched-mode power applications and resulting device stresses
- Demonstrated track record of commercially successful Power MOSFET developments
- Semiconductor Device Reliability Physics
- High Voltage VDMOS device engineering
- Power semiconductor device product development
- Product and test mask layout (preferably Cadence Virtuoso)
- Design of Experiments methodology
- Working familiarity with structural and chemical analysis for microelectronics
- Working familiarity with power device test and characterization equipment and methodologies
- Understanding of switched-mode power applications and resulting device stresses
ルネサスは、「To Make Our Lives Easier(人々の暮らしをより豊かで快適にする)」というPurposeのもと、組込み半導体ソリューションを提供するグローバル企業です。世界30か国以上で活躍する21,000人を超えるエンジニアや課題解決のプロフェッショナルとともに、自動車、産業、インフラ、IoT分野における世界最先端のテクノロジー開発に携わり、より安全で、健康的で、環境にやさしく、スマートな未来の実現に貢献しています。
ルネサスでは、「TAGIE(Transparent、Agile、Global、Innovative、Entrepreneurial)」を企業文化の中核としています。TAGIEは、私たちの働き方や成長のあり方、そしてPurposeの実現に向けた取り組みを支える共通の価値観です。この協調的な精神と挑戦するマインドセットが、半導体技術を通じた産業の変革と、世界中の人々の暮らしへの貢献を可能にしています。
私たちは、競争力のある報酬制度に加え、充実した福利厚生をご用意しています。福利厚生の詳細については、選考プロセスの中でご案内いたします。
私たちとともに未来を創造する挑戦に、ぜひ参加しませんか。皆さまからのご応募をお待ちしております。
- エンジニア
- 小平市
- No
求人ID
20024572_2026-01-06