Staff IT Analyst
Our company has been running a major project to consolidate the various systems, each with similar functionalities, that were used prior to past M&As into a single unified system.
This is essential to ensure smoother execution of future M&A activities.
At the same time, our company operates with systems that are closely integrated with production sites and contain advanced reporting functions, which also require adjustments and modifications as part of this integration.
【 Background of the recruitment】
The SCM planning systems also need to be consolidated into a single system.
This new solution will leverage a major packaged cloud-based system.
We are looking for personnel who can support the entire process of requirements definition, development, testing, user acceptance testing, and subsequent system maintenance and operations.
In addition, the role will serve as the main point of contact with production sites for system-related changes and will coordinate necessary adjustments.
We are seeking candidates who can support these system development activities as well as ongoing maintenance and operational tasks.
【Job details】
- Project management (requirements definition, development, testing, user testing, etc.) for the SCM planning system, which is our area within the overall system integration PJ.
- Requirement definition :
Coordination with planners from all over the world within the Renesas Group (business English conversation skills are necessary to discuss with members from Japan, Europe, and the U.S.) to compile the requirements for the system.
- Development, testing :
Customize PKG by ourself based on the system requirements definition.
If development outside of PKG is required, the vendor will be notified, and system review and user acceptance testing will be conducted after development is complete. Technical issues are also included with the development vendor (SQL, Java, etc.)
- System maintenance and operation work:
Responding to requests for improvement from business users during system operation and improvement activities for stable system operation, etc.
【Must】
・Experience in a series of operations such as demand management to production planning for about a few years.
・Experience with SQL DB operations and web system development languages (Java, etc.)
・Good for Communication Skills
・Japanese native level or N1
・Intermediate level of Business English
【Want】
・Advanced levell of Business English
ルネサスは、「To Make Our Lives Easier 」(人々の暮らしを楽“ラク”にする)というPurposeの下、組み込み半導体ソリューションを提供します。高品質とシステムレベルノウハウを兼ね備えた組み込み半導体のリーダーとして、自動車、産業、インフラ・IoT分野向けに、ハイパフォーマンスコンピューティング、組み込みプロセッシング、アナログ&コネクティビティ、そしてパワーを含めた幅広い製品ポートフォリオを軸とした、スケーラブルで包括的なソリューションを提供しています。
ルネサスは、30か国以上で22,000 人を超える多様性あふれる従業員と共に、限界に挑戦しながら、デジタライゼーションを通じてユーザエクスペリエンスを充実化させ、新たなイノベーションの時代を切り開いていきます。そして世界中の人々やコミュニティの未来のために、持続可能で省エネ効果の高いソリューションの開発に全力で取り組み、「To Make Our Lives Easier」を実現します。
ルネサスで実現できること
- キャリアをスタート、そしてキャリアアップ:4つのプロダクトグループをはじめ、さまざまな部門において技術職として、また幅広いビジネスの経験を積むことができます。ハードウェア、ソフトウェアの専門知識を深めたり、新しいことにチャレンジしたりする機会があります。
- やりがいとインパクトのある仕事をする: 革新的な製品とソリューションの開発に関わることにより、世界中のお客様のニーズに応えると同時に、人々の生活をより便利で安全かつ安心なものにすることに貢献できます。
- 「ウェルビーイング」に焦点を置いた環境で最大限に能力を発揮する:ルネサスでは、リモートワーク制度などによる柔軟な勤務体制づくり、また従業員リソースグループの積極的な活動をサポートするなど、インクルーシブな職場環境構築を目指しています。従業員を第一に考えたカルチャーとグローバルなサポート体制が、入社後すぐに活躍できる環境を提供します。
自分の力で成功を掴み、キャリアを築く準備はできていますか?
ルネサスで一緒に未来を形づくっていきましょう。
当社では、ハイブリッド勤務モデルを採用しており、従業員は週に2日間リモートワークを行うことができます。同時に、残りの日はチームとしてオフィスに集まり、協働を強化しています。出社指定日は火曜日から木曜日で、イノベーション、コラボレーション、そして継続的な学習に取り組む日としています。