JUMP TO CONTENT

Video IP / Subsystem Design Leader

この欠員は期限切れです。 下の同様の職務を参照してください...


Job Description

【Background of the Recruitment】

As vehicles become increasingly electrified and intelligent, automotive SoCs are now positioned as a central technology supporting vehicle performance and functionality.
The R-Car series has continued to grow as a large‑scale SoC through the advanced integration of numerous and diverse IPs, including CPU, memory, high‑speed interfaces, AI/video, functional safety, and security.
Our organization is responsible not only for in‑house IP development but also for the selection, integration, and implementation of external IPs, making the strengthening of technical leadership in core areas such as the Image processing subsystem a key focus.
Against this background, we are seeking technical leaders who can define design direction, make sound technical decisions, and move development forward in collaboration with surrounding teams and IP vendors.
This role offers an opportunity for engineers who wish to drive development with a strong technical foundation while preparing to take on broader responsibilities in the future.

【Job Description】

  • Play a key role in specification definition and architectural study of the Image processing subsystem for automotive SoCs (R-Car series).
  • Work on the Image processing subsystem including camera input and screen output image processing HW-IP and memory-related areas, and organize design directions from a subsystem-level optimization perspective while owning a primary technical area.
  • During logic design and verification phases, identify and structure technical issues, contribute to design decisions, and help drive development forward.
  • Consider constraints such as power, performance, and reliability, and make technical judgments consistent with overall SoC requirements.
  • For integrated third‑party IPs, communicate with IP vendors to confirm specifications, clarify constraints/assumptions, and support issue resolution.
  • Collaborate with design teams in India and Vietnam and with IP vendors, working in English within a global development environment.

※The full details regarding your position scope as well as any future potential changes in work location and job scope will be provided during the interview process.


Qualifications

【MUST】

  • Hands-on experience in at least one of the following areas, including specification study, design, verification, or performance evaluation:
    - Camera input image processing HW-IP (MIPI-compliant Video Interface, ISP (Image Signal Processor), DMA (Direct Memory Access), etc.)
    - Screen output image processing HW-IP (MIPI-compliant Video Interface, DisplayPort, DMA (Direct Memory Access), etc.)
    - Memory peripherals (interconnect, memory control, memory interface, etc.)
  • Ability to organize design directions and key discussion points based on requirements and share them with stakeholders.
  • Understanding of the logic design and verification flow, and experience actively participating in technical reviews/discussions.
  • Communication skills to collaborate across teams and contribute to technical consensus building.
  • Willingness and ability to communicate in English for technical meetings and specification reviews.

【WANT】

  • Experience taking a technical lead role at subsystem or IP level (e.g., leading design reviews, guiding technical discussions).
  • Experience in designing and verifying camera input and screen output.
  • Experience in image processing/image recognition IP (Intellectual Property) and SoC integration including memory.
  • Knowledge of power domain separation and physical implementation considerations (e.g., P&R).
  • Experience in automotive SoC development or design/verification with functional safety or reliability considerations.
  • Experience in technical communication and coordination with overseas sites and/or third‑party IP vendors.
  • Japanese language proficiency at a conversational level
     

Additional Information

If you are interested in this position, please feel free to contact us at the details below:
Recruiter:Masana Ueno

ルネサスは、「To Make Our Lives Easier 」(人々の暮らしを楽“ラク”にする)というPurposeの下、組み込み半導体ソリューションを提供します。高品質とシステムレベルノウハウを兼ね備えた組み込み半導体のリーダーとして、自動車、産業、インフラ・IoT分野向けに、ハイパフォーマンスコンピューティング、組み込みプロセッシング、アナログ&コネクティビティ、そしてパワーを含めた幅広い製品ポートフォリオを軸とした、スケーラブルで包括的なソリューションを提供しています。
 

ルネサスは、30か国以上で22,000 人を超える多様性あふれる従業員と共に、限界に挑戦しながら、デジタライゼーションを通じてユーザエクスペリエンスを充実化させ、新たなイノベーションの時代を切り開いていきます。そして世界中の人々やコミュニティの未来のために、持続可能で省エネ効果の高いソリューションの開発に全力で取り組み、「To Make Our Lives Easier」を実現します。    
 

ルネサスで実現できること
 

  • キャリアをスタート、そしてキャリアアップ:4つのプロダクトグループをはじめ、さまざまな部門において技術職として、また幅広いビジネスの経験を積むことができます。ハードウェア、ソフトウェアの専門知識を深めたり、新しいことにチャレンジしたりする機会があります。 
     
  • やりがいとインパクトのある仕事をする: 革新的な製品とソリューションの開発に関わることにより、世界中のお客様のニーズに応えると同時に、人々の生活をより便利で安全かつ安心なものにすることに貢献できます。
     
  • 「ウェルビーイング」に焦点を置いた環境で最大限に能力を発揮する:ルネサスでは、リモートワーク制度などによる柔軟な勤務体制づくり、また従業員リソースグループの積極的な活動をサポートするなど、インクルーシブな職場環境構築を目指しています。従業員を第一に考えたカルチャーとグローバルなサポート体制が、入社後すぐに活躍できる環境を提供します。 

 

自分の力で成功を掴み、キャリアを築く準備はできていますか? 

ルネサスで一緒に未来を形づくっていきましょう。

当社では、ハイブリッド勤務モデルを採用しており、従業員は週に2日間リモートワークを行うことができます。同時に、残りの日はチームとしてオフィスに集まり、協働を強化しています。出社指定日は火曜日から木曜日で、イノベーション、コラボレーション、そして継続的な学習に取り組む日としています。

  1. エンジニア
  2. 小平市
  3. No

求人ID

11015276_2026-03-02

職種検索

Browse Jobs